Technical FAQs

Ask a Question

What size ring terminal can be used on the Masterpact NW ring terminal accessory connections?

Issue:
What size ring terminal can be used on the Masterpact NW ring terminal accessory connections?   What is the ring terminal screw diameter and maximum OD (outside diameter) of the ring terminal that can be used on the Masterpact NW Ring terminal accessory connections? 

Product Line:
Masterpact NW

Resolution:
Ring terminal screw diameter: 0.1325 inch
Connector interior width/max ring OD: 0.306 inch.
Wire size: 22 to 14 AWG

 
Was this helpful?
What can we do to improve the information ?