Technical FAQs

Ask a Question

On and NF or NQ panelboard, what material are the bus connectors?

Issue:
Bus finger composition

Product Line:
Panelboards

Environment:
NF

Cause:
Material content

Resolution:
The bus connectors on a NF or NQ panel are copper regardless of the bus being copper or aluminum.


CTA-ID : 2054069
Was this helpful?
What can we do to improve the information ?