Technical FAQs

Ask a Question

Can he directly connect a 4 pole LC1DT32F7 to a GV starter with a GV2AF4.

No, not directly. Though the 3 pole and 4 pole are the same width physically, the spacing between the terminals are different on a 4 pole and 3 pole. The prongs on the GV2AF4 are spaced for a 3 pole, not a 4 pole.


CTA-ID : 2055620
Was this helpful?
What can we do to improve the information ?