Technical FAQs

Ask a Question

What is the inrush and sealed VA for an LC1F780 contactor coil?

40 - 400 Hz coil - 2100 VA Inrush, 50 VA sealed @ 50 or 60 Hz.



CTA-ID : 2054959
Was this helpful?
What can we do to improve the information ?