Technical FAQs

Ask a Question

What are the repair parts for a CHU366R Series E2 and E4 Heavy Duty Safety Switch?

Issue:
Previous Design Repair parts

Product Line:
Heavy Duty Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:

NOTE: This is a Non-Fusible Switch so it does NOT have a Separate Load Base Assembly.
The parts listed here are the only field replaceable parts.

Complete interior - HUN366E2 (includes line base assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line/Load base assembly - 4055218650SEL (3-required and arc suppressor assembly is not included)
Arc suppressor assembly - 4051270850 SEL (3-required) (OBSOLETE replaced by 4051270850)
Lug assembly - 4405044601 (2 required per base assembly)
Line base phase insulator - 4055219301 (2 required)
Line base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250 SEL
Door thumb retainer - 4405049001 (2 required)
Door thumb screw - 4405043401 (2 required)
Handle knob kit - 4028343550 (the black & red knob at the end of the handle)


 
Was this helpful?
What can we do to improve the information ?