Technical FAQs

Ask a Question

Can I get a weld control contactor class 8990D01? It goes on a spot welder.

This contactor is obsolete. It is from the `40s, 50`s or 60`s. Referred to Precision Contactor Co. 575-885-5069. They rebuild these old contactors.

CTA-ID : 2055499
Was this helpful?
What can we do to improve the information ?