Technical FAQs

Ask a Question

Can you get control wire taps for the Powerpact L breaker? Control wire kit?

Issue:
Can you get control wire taps for the Powerpact L breaker? Control wire kit?

Product Line:
Powerpact L frame

Environment:
Mechanical Lugs

Cause:

Resolution:
Yes, control wire taps come standard with the L frame lugs, but the screw does not. For control wire installation, use an 8-32 x 1/4 in. screw (not provided) into tapped control wire hole in lower left hand corner of lug.


CTA-ID : 2059521
Was this helpful?
What can we do to improve the information ?