Technical FAQs

Ask a Question

Which type of lighting contactor has latch and unlatch coils, the electrically held or the mechanically held?

Issue:
Which type of lighting contactor has latch and unlatch coils, the electrically held or the mechanically held?

Product Line:
NEMA Lighting Contactors

Environment:
Products sold and used in the United States

Cause:
Which type of lighting contactor has latch and unlatch coils, the electrically held or the mechanically held?

Resolution:
Mechanically held has latch and unlatch coils. The electrically held only has a single coil.





CTA-ID : 2059479
Was this helpful?
What can we do to improve the information ?