Technical FAQs

Ask a Question

What does the QO3125SL do for a QO panel?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The QO3125SL is a 3 pole, 125A rated subfeed lug kit designed to allow the user the ability to subfeed to a subpanel. It is branch mounted and will require 3 spaces in the 3 phase load center. It has no overcurrent protection.


CTA-ID : 2060125
Was this helpful?
What can we do to improve the information ?