Technical FAQs

Ask a Question

What are the repair parts for UFP222RNM, Series G01, AC Disconnect?

Issue:
Repair parts

Product Line:
AC Disconnect

Environment:
All Fusible or not fusible ac disconnect with pullout head

Cause:
Maintenance

Resolution:
NOTE: Pullout part number 4050711750 is obsolete and no longer available. There is no replacement.
Only the parts listed below are considered field replaceable (for pictures see attached link):
Interior Trim - Cannot be provided due to UL labeling issues.
Pullout - 4050711750 (This pullout will work for either Series G01 or G02) (OBSOLETE - NO LONGER AVAILABLE - NO REPLACEMENT)
Interior Trim Mounting Screw  - 2153310141


CTA-ID : 2056706
Was this helpful?
What can we do to improve the information ?