Technical FAQs

Ask a Question

Does the ATV312 have a display value that can be customer defined and scaled to correspond to machine speed, process speed or motor speed?

Issue:
Does the ATV312 have a display value that can be customer defined and scaled to correspond to machine speed, process speed or motor speed?

Product Line:
ATV312 Drives

Environment:
All serial numbers for ATV312 Drives

Cause:
N/A

Resolution:
Yes.
The display code SPd1 or SPd2 or SPd3 is for the output value in customer units.  These code values depend on the SdS parameter.  See the BBV46385 Programming manual for details.  Factory setting is SPd3.
SdS is the scale factor for the display parameter.  It is used to scale a value (such as motor speed) in proportion to the output frequency rFr.


 
Was this helpful?
What can we do to improve the information ?