Technical FAQs

Ask a Question

In a Canadian Meter center, is it possible to size a bus bar system of 1000 Amp with MCMBK600 + MCMBK400?

No, the bus system should be sized using 2x MCMBK600 connector bus bars per phase.


CTA-ID : 2060292
Was this helpful?
What can we do to improve the information ?