Technical FAQs

Ask a Question

What is the part number for the neutral lug on Canadian Meter Centers MC54L3 & MC54L?

The lug is secured to the neutral bus bar with a screw and flat-washer.
The required parts are Neutral Lug is part number L79A486 , Screw part number 11721SJ3/4 and flat washer 23601-00200.
One of each is required per sub-service (total of 3 for the MC5-4L3 or total of 6 for the MC5-4L meterstack).



CTA-ID : 2060312
Was this helpful?
What can we do to improve the information ?