Technical FAQs

Ask a Question

What is the 480 volt replacement coil for an 8502A Series B or C Contactor?

The coil numbers were 31012-400-61 for 60hz and 31012-400-64 for 50 hz. Both of these coils are obsolete and no longer available. Series A coils are also obsolete and no longer available. This also applies to all 8536A, 8702A, 8736A and 8810A, devices. For enclosed devices, the series information is based on device and not enclosure nameplate.


CTA-ID : 2060717
Was this helpful?
What can we do to improve the information ?