Technical FAQs

Ask a Question

Can you do a multipoint addressing with the ATV312 drives?

Issue:
Can you do a multipoint addressing with the ATV312 drives?

Product Line:
Altivar ATV312

Environment:
All

Cause:
Needs to set up an Multipoint addressing on the ATV312 drive.

Resolution:
   It is not possible to do multipoint addressing with the ATV312 drives.  The menu for the configuration can be displayed on the remote HMI  but it is not a working function of the drive because the function has not been implemented.  If you want this feature you will need to use the ATV61 or ATV71 drives.
Was this helpful?
What can we do to improve the information ?