Technical FAQs

Ask a Question

Do we have an enclosure for Powerpact H and J frame breakers with Micrologic trip units?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosure

Cause:
Product features

Resolution:
The H- and J-frame circuit breakers with electronic trip units can be unit mounted in the J250F, J250AWK, or J250R enclosures.
Limitations are:  
>No communication capabilities will be available (no Interface Module or Front Display Module), and
>The trip unit will not be accessible or visible without the removal of the cover


CTA-ID : 2061138
Was this helpful?
What can we do to improve the information ?