Technical FAQs

Ask a Question

What is the replacement handle part number for a Class 2601 Type AG2 reversing drum switch?

Issue: What is the replacement handle part number for a Class 2601 Type AG2 reversing drum switch?

Product Line: 2601 reversing drum switches

Environment: Products sold and used in the United States

Cause: Replacement handle needed for a 2601AG2 drum switch

Resolution: One piece standard plastic handle - 2917-A5-X1 or
Optional ball and shaft handle - OBSOLETE or
Optional fluted handle - OBSOLETE
Replacement mounting screw - not available suggest obtaining 8-32 x 1/4``.


CTA-ID : 2060786
Was this helpful?
What can we do to improve the information ?