Technical FAQs

Ask a Question

How can you set up the ATV32 drives to utilize the multipoint configuration with one HMI?

Issue:
How can you set up the ATV32 drives to utilize the multipoint configuration with one HMI?

Product Line:
Altivar 32

Environment:
All

Cause:
ATV32 setup multipoint configuration with one HMI

Resolution:
You must assign each ATV32 drives modbus address between 1 thru 247.
Goto: FULL menu
Goto: CON menu
Goto: nd1 menu
Add= Modbus address
tbr= Modbus baud rate
tFO= Modbus Format
ttO= Modbus time out

See attached file for connection examples.

See attached file for Multipoint Screen access menu examples.

 
Was this helpful?
What can we do to improve the information ?