Technical FAQs

Ask a Question

Do we have a way to field modify the Eflex drive to have an end of damper control?

Issue:
Do we have a way to field modify the Eflex drive to have an end of damper control?

Product Line:
8839 E-Flex

Environment:
All

Cause:
Needs to add a damper control circuit to an enclosed E-Flex drive.

Resolution:
The E-Flex install manual shows a addition of a 8501 relay if you order the Eflex drive with mod S09 from the factory.  However there is a 2nd way of adding the end of damper option in the field.
 
Using the old Econoflex Field installed diagram you can rewire the Eflex control wiring diagram the same way to get the end of damper option without having to add the 8501 relay.

See the attached file for an example of the wiring diagram.



 
Was this helpful?
What can we do to improve the information ?