Technical FAQs

Ask a Question

What size contactors are recommended for use with an ATS48C17Y?

For standard duty applications:
Use the LC1F150 for an Isolation Contactor, Shorting Contactor or Reversing Contactor.
Use the LC1F185 for a full voltage bypass contactor.
Order the coil separately based on control voltage.

CTA-ID : 2061968
Was this helpful?
What can we do to improve the information ?