Technical FAQs

Ask a Question

What will the display on ATV212 show when a logic input is programmed for run permissive and the input is open?

Issue:
What will the display on ATV212 show when a logic input is programmed for Run permissive and the input is open?

Product Line:
Altivar ATV21 and ATV212

Environment:
All

Cause:
run permissive is open

Resolution:
It will show display status of  OFF.

Was this helpful?
What can we do to improve the information ?