Technical FAQs

Ask a Question

What is the difference between the ET1.0I and Micrologic trip units?

Product Line:
Circuit Breakers
PowerPact P, and R
Masterpact NW, and NT

Environment:
Electrical Distribution Equipment

Resolution:
ET1.0I  is a fixed amperage non interchangeable trip unit.  Has instantaneous adjustments.

The Powerpact P, R and Masterpact Micrologic is an adjustable amperage, field interchangeable trip unit.  Options include digital display and advanced features like power, energy, harmonics, and modbus communications.


CTA-ID : 2062571
Was this helpful?
What can we do to improve the information ?