Technical FAQs

Ask a Question

What are the Micrologic 5.0P ground fault alarm pick up and delay ranges?

Issue:
What are the Micrologic 5.0P ground fault alarm pick up and delay ranges?

Product Line:
Microligic 5.0P, 6.0P, 5.0H and 6.0H

Environment:
Trip units that go on Powerpact P, R; and Masterpact NW and NT

Cause:
Programming the GF alarm pick up values

Resolution:

Pickup: 0.1 x In to In  (In = Sensor size).   Floor is 120 amps and Ceiling is 1200 amps, +/- 15%.
Delay:  1 to 10 seconds, -20%, +0%

Drop out: 0.1 x In to Pickup.  Floor is 120 amps and Ceiling is Pickup. (Drop out cannot be set higher than Pickup.),   ±15%
Dropout Delay:  1 – 10 sec.,  -20%, +0%

 
Was this helpful?
What can we do to improve the information ?