Technical FAQs

Ask a Question

How can you configure the ATV32 drive to use assemblies 20/70 and 21/71?

Issue:
How can you configure the ATV32 drive to use assemblies 20/70 and 21/71?

Product Line:
Altivar ATV32

Environment:
ATV32 with Ethernet option card installed

Cause:
Set up configuration to use assemblies 20,21,70 and 71.

Resolution:
See case #2 example in the following attachment.
 

Was this helpful?
What can we do to improve the information ?