Technical FAQs

Ask a Question

On an E-Flex, what is modification B09?

This option provides a line contactor factory wired between the circuit breaker disconnect ( or line reactor when provided ) and the ATV61 power converter. It provides full isolation of the ATV61 when the EFlex is running in BYPASS mode.

Not available with Nema 3R enclosures.
Not compatible with power circuit W ( without bypass ).

CTA-ID : 2062787
Was this helpful?
What can we do to improve the information ?