Technical FAQs

Ask a Question

Do the ATS22 products have an internal contactor?

Yes.  It is a shorting contactor that closes when the motor is up to full speed.  The purpose is to give the current a path around the SCRs.  This prolongs the life of the SCRs.  Note that this contactor is not for full voltage starting.

CTA-ID : 2062527
Was this helpful?
What can we do to improve the information ?