Technical FAQs

Ask a Question

Is there a 208Vac, 240Vac or 277Vac shunt trip for the J frame breaker?

Issue:
Is there a 208 V, 277 V or 240 V shunt trip for the PowerPact J-frame breaker?

Product Line:
PowerPact J Frame

Environment:
This applies to all PowerPact J frame breakers both unit mount and I-Line including Thermal-magnetic and Electronic trip.

Cause:
Need to trip a J frame breaker with a control voltage of 240Vac.

Resolution:
Yes use either SD as a suffix or order S29387.
Was this helpful?
What can we do to improve the information ?