Technical FAQs

Ask a Question

What is the replacement for the Compact CK1200 circuit breaker?

Product Line:
CK1200 Circuit Breakers

Resolution:
The Compact CK1200 is a general description for a line of circuit breakers. These were sold under the name of Merlin Gerin, which was acquired by Schneider Electric in 1992. The Compact CK1200 line of circuit breakers includes many different actual catalog numbers.

Regarding availability, the Compact CK1200 Circuit Breakers are obsolete and no longer available. If necessary to replace an existing CK1200, a currently-produced circuit breaker can be used that will perform the same function. It is very important to note, however, that the new replacement circuit breaker will be of different size and mounting dimensions compared to the Compact CK1200. The terminals and accessories will also be different. To help clarify dimensions and ratings of the obsolete CK1200 circuit breakers, see the attached two files.

When choosing the replacement circuit breaker, there may be several possibilities from which to choose. Our online Digest includes much of this information (click this link). To speak with someone, call us at 888-778-2733, and ask for Technical Support for Circuit Breakers.

Was this helpful?
What can we do to improve the information ?