Technical FAQs

Ask a Question

Need 1P, 2P or 3P wiring diagram / Installation Bulletin for QO or QOB GFI breakers.

Issue:
Need 1P, 2P or 3P wiring diagram / Installation Bulletin for QO or QOB GFI breakers.

Product Line:
QO-GFI, QOB-GFI

Environment:
This applies to all QO and QOB GFI breakers

Cause:
Need the correct wiring diagram for the QO or QOB GFI breaker.

Resolution:
  • 1P: Refer to Instruction Bulletin 48840-088-01.
  • 2P: Refer to Instruction Bulletin 48840-435-03.
  • 3P: Refer to Instruction Bulletin 48840-260-01.
These documents can be found in the Schneider Electric Technical Library.
Was this helpful?
What can we do to improve the information ?