Technical FAQs

Ask a Question

Is there any other auxiliary contact module for the LC1D80BD other than the LADN modules?



Issue:

Is there any other auxiliary contact module for the LC1D80BD other than the LADN modules?

Auxiliary contacts are needed but there isn't any additional front clearance.

Product Line:
Tesys D

Environment:
Products sold and used in the United States
 
Resolution:

There is no way to side mount an aux contact on the DC coil version of the LC1D80 device.
Only the 1 normally open and 1 normally closed auxiliary contact that is provided with the device may be used.


Was this helpful?
What can we do to improve the information ?