Technical FAQs

Ask a Question

What is the dissipated heat on the ATS22C48S6U soft starter?

Issue:
What is the dissipated heat on the ATS22C48S6U?

Product line:  
Altistart 22

Environment:
ATS22C48S6U

Cause:
Excessive power dissipation can cause overheating   

Resolution:
Refer to the ATS22 User Manual. 
The power dissipation at steady state is 144 watts. 
Was this helpful?
What can we do to improve the information ?