Technical FAQs

Ask a Question

Where can you find the Modbus and cable drivers for TCSMCNAM3M002P USB cable?

Issue:
Where can I get the TCSMCNAM3M002P device driver and modbus drivers for Windows

Product line:
Altivar, Altistart

Environment:
All models, all serial numbers;

Cause:
Cannot connect to the unit.  Does not have the correct Modbus driver

Resolution:
The Modbus driver can be downloaded by clicking this link.  The file will be listed.
Below are the links from our FTP Site to the latest drivers for the TCSMCNAM3M002P cable. The software is free online, however, you will need to purchase this cable to connect your PC to products via the resident Modbus port.

TCSM CABLE Driver: http://www.schneider-electric.com/en/download/document/TSXCUSB+and+TCSMCNAM+DRIVER/

You may also need one of these depending on what operating Windows 7 system you have.
Modbus Driver 32bit;  https://schneider-electric.box.com/Modbus-Driver
Modbus Driver 64bit;  https://schneider-electric.box.com/Modbus-64bit
 
Note if you are using SoMove version 2.021 or higher the modbus driver is installed in the SoMove software so you do not have to download the Modbus driver files.
Was this helpful?
What can we do to improve the information ?