Technical FAQs

Ask a Question

What is the part number for the replacement lug cover for an LC36600?

Product Line:
Legacy Circuit Breakers

Environment:
Electrical Distribution Equipment
LC LCL LI LIL

Resolution:
Replacement cover part number is 48140-044-01. This has to be ordered through Cedar Rapids Customer Service.
Advise customer to order two screws (21507-17243) also as they do not come with the above number.  The cover label is not available.


 
Was this helpful?
What can we do to improve the information ?