Technical FAQs

Ask a Question

Is a replacement enclosure only available for a safety switch?

ISSUE:
The Safety Switch enclosure has been damaged and needs to be replaced.

PRODUCT LINE :
Safety Switches

ENVIRONMENT:
Applies to  NEMA Type of safety switch enclosures

CAUSE:
An installed Safety Switch has been damaged, and the customer needs wants a replacement enclosure to repair the switch.

RESOLUTION:
Replacement enclosures only are not available. The labeling provided on a safety switch cover includes the UL Mark. The UL Mark can only be applied to a complete switch as it was tested and listed. Therefore, a replacement enclosure, or cover, cannot be provided. The complete switch would need to be replaced.
Was this helpful?
What can we do to improve the information ?