Technical FAQs

Ask a Question

What is the Torque requirement for the Main Lugs of the DU324RB?

Issue:
Main Lug Torque requirements.

Product line:
General Duty Safety Switches

Environment:
Applies ONLY to the Main(Line, Load & Neutral) Lugs for a DU324RB General Duty Safety Switch.  

Cause:
Torque required for the Installation of the Main wires into the line, load & Neutral  lugs of the safety switch.

Resolution:
The torque requirements are located on the wiring diagram of the safety switch. The wiring diagram is located on the back side of the front cover. The Torque value shown on the wiring diagram for the Line, Load and Neutral Main lugs is 275 lbs-in Max.
Was this helpful?
What can we do to improve the information ?