Technical FAQs

Ask a Question

Do we have a lug for 600 kcmil for the Powerpact L 400A and 600A breaker?

ISSUE
Customers want to use one 600 kcmil conductor instead of two smaller conductors with this breaker

PRODUCT LINE
Powerpact L

RESOLUTION
Yes, lug kit AL400L61K3 will accept wire range(1) 2 AWG–500 kcmil Al or (1) 2 AWG–600 kcmil Cu.  The kit contains 3 lugs per kit.
Was this helpful?
What can we do to improve the information ?