Technical FAQs

Ask a Question

How to separately mount the LRD350

Issue:
Method of mounting the LRD350 by itself in a panel

Product Line:
Overload relays

Environment:
IEC style bimetallic overload relays

Cause:
The overload is not to be mounted directly to the contactor but mounted separately on the panel

Resolution:
The LRD350 is din rail mountable on it's own. To make the overload independently or separately mounted you need an Everlink terminal block (LAD96560) to snap on top.
Was this helpful?
What can we do to improve the information ?