Technical FAQs

Ask a Question

Can 9422 TG2 be furnished with provisions for (2) 250kcmil?

Issue:
Can 9422 TG2 be furnished with provisions for (2) 250kcmil?

Product Line:
Fusible switch operating mechanisms

Environment:
Class 9422 Type T Fusible switch operating mechanisms

Cause:
Product features

Resolution:
Yes, a second lug can be added that will accept a #4 to 350kcmil.  The part number is 2505044601. There is an anti rotation spacer that will need to be removed to add the new lug.

 
Was this helpful?
What can we do to improve the information ?