Technical FAQs

Ask a Question

Can auxiliary switches be field installed on the H225XJG?

Issue:
Can auxiliary contacts be field installed on the H225XJG? 
 
Product Line:
Enclosed Molded Case Switches

Environment:
Applies to the H225XJG only

Cause:
Clarification

Resolution:
The molded case switch provided in the H225XJG is a JGL36000S25, which will accept field installed auxiliary contacts. Order part number S29450 for 1 NO and 1 NC contacts. Up to two S29450 can be installed.
Was this helpful?
What can we do to improve the information ?