Technical FAQs

Ask a Question

Is it normal for an 8910DPA24V02 definite purpose contactor to be "chattering" during normal use?

Issue:
Is it normal for an 8910DPA24V02 definite purpose contactor to be "chattering" during normal use?

Product Line:
NEMA definite purpose contactors

Environment:
Class 8910 definite purpose contactors

Cause:
Application

Resolution:
This behavior can be expected when using a definite purpose contactor. These should be used in applications where noise suppression is not needed.
 

Was this helpful?
What can we do to improve the information ?