Technical FAQs

Ask a Question

How is the ATV312 programming returned to the factory defaults?

Issue:
ATV312 needs to be set back to the original factory settings.

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
None

Resolution:
Use the following steps to reset the ATV312 to factory settings:
From the default display, press Enter
Turn to menu drC, press Enter
Turn to parameter FCS, press Enter
Turn to setting InI, press and hold Enter for 2 seconds
Was this helpful?
What can we do to improve the information ?