Technical FAQs

Ask a Question

What is the part number for an adapter plate kit for the ATS46 to ATS48 conversion?

Issue:
When replacing an ATS46 with an ATS48, is there a mounting plate adapter available?

Product line:
Altistart ATS48

Environment:
All models, all serial numbers

Cause:
Retrofitting an ATS48 in place of an ATV46

Resolution:
There is no adapter plate option to facilitate the conversion.
Was this helpful?
What can we do to improve the information ?