Technical FAQs

Ask a Question

Does the 3107440038 coil bolt in?

ISSUE
Does the 31074-400-38 coil bolt in?


PRODUCT LINE
NEMA size 3 contactors


ENVIRONMENT
NEMA size 3 contactors sold in the US


RESOLUTION
The coil itself does not bolt in, but the steel core which sits inside the coil must be bolted in to seat the coil.
Was this helpful?
What can we do to improve the information ?