Technical FAQs

Ask a Question

What is the part number for the 480V replacement coil for a T02DN13?

Issue
What is the part number for the 480V replacement coil for a T02DN13?

Product
TeSysN NEMA rated contactors and Starters (Blend of TeSys and Type S devices)

Environment
T02DN13, TesysN, LC1D65A, NEMA Size 2

Cause
Replacement coil

Resolution
The T02DN13 is a NEMA rated size 2 LC1D65A contactor. The part number for the 480 VAC replacement coil is LXD3T7.  
  

Was this helpful?
What can we do to improve the information ?