Technical FAQs

Ask a Question

How does the cable-connected Powerpact L frame breaker mount in an enclosure?

Product Line:
Powerpact LDL LGL LJL LLL LRL

Cause:
Customers sometimes buy third-party enclosures for Powerpact L breakers

Resolution:
The Powerpact L frame breaker comes with four screws, nuts, and washers for mounting the breaker to a backplate.  The nuts and washers go behind the backplate. 
It may also be mounted to a threaded backplate.  The screws are M5 x 85 (mm).
 

Was this helpful?
What can we do to improve the information ?