Technical FAQs

Ask a Question

Does a 9065SF020 provide the same mounting capabilities as the 9065SF120 for an 8536SCOVO2H21S starter?

Issue:
When mounting an overload for the for an 8536 starter, does interchanging an SF020 and SF120  solid state overload change the mounting capabilities? does this cause an issue with the looping of the power wires.

Product Line: 
Full Voltage Starters NEMA style, Thermal overload relays

Environment:
Unique to the 8536. 3 pole NEMA Starters 00b-4( seperate mounting)  Includes all the features on the Base Unit

Cause:
Looping of wires

Resolution
Mounting capabilities of the 9065SF020 and the 9065SF120 are essentially the same for the seperate mounting or direct mounting of the overload relay.
Was this helpful?
What can we do to improve the information ?