Technical FAQs

Ask a Question

Where do you terminate the load side conductors to the 9065 motor logic solid state overload relay in the Nema size 00,0, and 1 8536 starters?

Issue:
Where do you terminate the load side conductors to the 9065 motor logic solid state overload relay in the Nema size 00,0, and 1 8536 starters?

Product Line:
Full Voltage starters NEMA style, Solid State overload relays

Environment:
8536, 9065 motor logic

Cause:
Assembly/wiring
 
Resolution:

Run the conductors from the motor up through the CT's on the bottom of the 9065 solid state motorlogic overload relay,
Terminate the conductors to the bottom of the contacts labeled T1 T2 AND T3 located at the bottom of the contactor. 

Was this helpful?
What can we do to improve the information ?