Technical FAQs

Ask a Question

What is the part number for the starter only for a 8538SCA22***?

Issue:
What is the part number for the standard starter with a melting alloy overload relay for a 8538SCA22***?  
Product Line:
Combination Starters
Environment:
8538 Fusible combination starter
Cause:
Maintainance and repair, product features
Resolution:
The standard starter with a melting alloy overload relay is 8536SCO3***.
To complete the starter part number a coil voltage code is required. V01, V02, V06 etc...
Was this helpful?
What can we do to improve the information ?