Technical FAQs

Ask a Question

Can multiple motor leads be wired in the same conduit?

Issue: 
Can multiple motor leads be wired in the same conduit?

Product Line:
All Altivars

Environment:
All

Cause: 
Multiple motor and or Line leads from different drives in the same conduit.

Resolution:
It is not recommended to run the motor leads from different drives in the same conduit. 
Multiple motor leads from different drives is not recommended because the noise generated from the pulse width modulated (PWM) waveform can cause cross-talk resulting in possible nuisance tripping.

Was this helpful?
What can we do to improve the information ?