Technical FAQs

Ask a Question

What are the wire or cable sizes required for the GV7RE and GV7RS starters?

Issue:
What are the wire or cable sizes required for the GV7RE and GV7RS starters?

Product Line:
Manual starters and protectors

Environment:
Tesys GV2,GV3 and GV7

Cause:
Wiring and installation of starters

Resolution:
For the GV7R*20 thru R*150 use a mechanical lug kit / clip-on connectors for 1 #14-3/0 GV7AC021 (sold in lots of 3) . For the GV7R*220 use a kit for 1 #14-350mcm GV7AC022 (sold in lots of 3).
Was this helpful?
What can we do to improve the information ?